Technical FAQs

Ask a Question

What are the repair parts for the HU664AWK, series F5? (may be shown as F05)

The repair parts for the HU664AWK, series F5 (F05) are as follows. No other parts are available.
Complete Line/Load Base (all one piece) - 4056704350 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line/Load Base mounting screws - 40205-464-01 (requires 12 per line base)
Arc Suppressor Assembly - 40566-775-50 (requires one per phase)
Arc Suppressor mounting screw - 40205-145-01
Lug Assembly - 40251-162-51 (per lug)
Lug Assembly mounting screw - 21401-222-40
Switch Mechanism - 40567-401-50 (requires Interlock Shaft Gasket 40567-860-01)
Switch Mechanism mounting screws- 22999-405-62 (requires 2)
Handle Assembly - 40567-468-50 (requires handle gasket 40566-031-01)
Lockplate - 40567-467-01
Lockplate mounting screws - 22999-405-62 (requires 2)



CTA-ID : 8967
Was this helpful?
What can we do to improve the information ?