Technical FAQs

Ask a Question

Can a Modulator Combiner Hub, catalog number SDM81VC, be cascaded to provide more than the eight modulator inputs provided?

Yes. Any one, or up to all eight, of the modulator input ports on a ``master`` SDM81VC may be connected to the output port of ``expansion`` Combiner Hubs. If all eight modulator input ports of the ``master`` Combiner Hub were connected to output ports of eight ``expansion`` Combiner Hubs, a total of 64 modulator inputs would then be available.
* No further cascading from the modulator inputs of the ``expansion`` Combiner Hubs.
* All Modulator Combiner Hubs must be powered.

CTA-ID : 2183
Was this helpful?
What can we do to improve the information ?