Technical FAQs

Ask a Question

Can multiple Video Amplifier Hubs, SDM16VAB, be used to provide more than six output signals to television locations?

Yes. The SDM16VAB is provided with two ``Long`` outputs (max 150` coax runs) and four ``Short`` outputs (max 75` coax runs). Any one, or all four, of the ``Short`` outputs could be used to connect to other SDM16VAB input ports.
* DO NOT use the ``Long`` outputs to cascade to other amplifiers.
* The maximum outputs, based on using all four ``Short`` outputs of the primary amplifier to feed four secondary amplifiers inputs, would be 26 (10 ``Long`` 150` max runs and 16 ``Short`` 75` max runs).

CTA-ID : 2140
Was this helpful?
What can we do to improve the information ?