Technical FAQs

Ask a Question

What is the acceptable mounting positions for the NEMA 8536 Type S devices?

Issue:  
What is the acceptable mounting positions for the NEMA 8536 / 8502 Type S devices?

Product Line:
NEMA Starters and Contactors

Environment:
Products sold and used in the United States

Cause: 
Installation
 
Resolution:
NEMA sizes 00 through 7 can be mounted vertically in the vertical plane. Class 8903 30-800 amp electrically held, and all class 8903 mechanically held, lighting contactors may also be mountedertically in the vertical plane.

 
Was this helpful?
What can we do to improve the information ?