Technical FAQs

Ask a Question

I need a ground fault system for a PCF breaker. Is the ground fault shunt trip field installable?

The ground fault shunt trip is factory installed only. However, the ground fault shunt trip is only used with the obsolete GP GROUND-CENSOR system and the MICROLOGIC add on ground fault modules. The GC-100, GC-200 and GA ground fault systems use a 120Vac shunt trip.


CTA-ID : 1923
Was this helpful?
What can we do to improve the information ?