Technical FAQs

Ask a Question

Does the 25hp 460V Class 8839 Altivar 58 Econo-flex power converter have an internal reactor as a standard feature?

The Class 8839 Altivar 58 Econo-flex July 2000 Instruction Bulletin 30072-450-10D lists the 25hp 460 V Econo-flex with a FLEX58D28N4 power converter. This power converter did have a internal line reactor as standard.

Hp rating changes occurred on the Econo-flex 460V AC drives as given in the Class 8839 Altivar 58 Econo-flex May 2001 Instruction Bulletin 30072-450-10E. This bulletin lists the 25hp 460V Econo-flex power converter as FLEX58KD23N4. This power converter does not have an internal reactor. A line reactor now needs to be ordered as an A09 miscellaneous option.


CTA-ID : 1762
Was this helpful?
What can we do to improve the information ?