Technical FAQs

Ask a Question

Is there a mechanical interlock for the QOU350?

Yes. You can interlock a 1 or 2 pole low-amp QOU breaker with a 2 or 3 pole low-amp QOU breaker. Catalog number: QOU2DTILA.

CTA-ID : 2430
Was this helpful?
What can we do to improve the information ?