Technical FAQs

Ask a Question

What considerations should he use when sizing the Altistart ATS46 softstart?

Told him the number of starts per hour, load type such as high inertia or not, motor FLA and application.


CTA-ID : 7493
Was this helpful?
What can we do to improve the information ?