Technical FAQs

Ask a Question

Is the fault relay on the Altivar ATV18 programmable?

Issue: Is the fault relay on the Altivar ATV18 programmable?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: The relay is not programmable--it is used as a fault relay. However the logic output can be assigned to speed reference attained or frequency level attained.


 
Was this helpful?
What can we do to improve the information ?