Technical FAQs

Ask a Question

Why does Altivar ATV18 drive not start when has a contact closure between LI1and +24 to start?

May not have a speed reference. Set the Low speed to the desired operating range and without a speed reference it will run at this value..


CTA-ID : 4346
Was this helpful?
What can we do to improve the information ?