Technical FAQs

Ask a Question

Is it ok to run single phase power on a three phase Altivar ATV18 unit?

We do not recommend or support this and even if oversize the ATV18 the normal 40% for single phasing you run the risk of damaging the unit because the filter circuit in it is more succetable to failure due to this incorrect usage.

CTA-ID : 4314
Was this helpful?
What can we do to improve the information ?