Technical FAQs

Ask a Question

Where is the date code located on an open style Altivar ATV18 drive?

Issue:  Where is the date code located on an open style Altivar ATV18 drive?
 
Product Line:  ATV18
 
Environment:  All
 
Cause:  N/A
 
Resolution:  On the lower right hand corner, it is a 4 digit number on white sticker.


 
Was this helpful?
What can we do to improve the information ?