Technical FAQs

Ask a Question

Can I use a 2-pole gfi for two single circuits?

Yes. However, the two circuits must have a common neutral which attaches to the load neutral connection on the breaker.


CTA-ID : 6155
Was this helpful?
What can we do to improve the information ?