Technical FAQs

Ask a Question

What does the customer do to get the additional contact on the selector switch on the enclosed Altistart ATS46?

Told him the can enter it as a SPL on the order and spell out how many and what function they want them on, or since we use the ZBA type deviceses, the can order interlocks and add them in the field.

CTA-ID : 7427
Was this helpful?
What can we do to improve the information ?