Technical FAQs

Ask a Question

Can you use a keypad at same time using Modbus on the Altistart ATS46?

No, you can not have a keypad as well because the PLC Communication Module VW3G46301U plugs into the keypad port.

CTA-ID : 7494
Was this helpful?
What can we do to improve the information ?