Technical FAQs

Ask a Question

Can the shorting contactor be used as a bypass contactor on the Altistart ATS46?

Could not route wiring through the softstart as done with shorting contactor. When in bypass would need to isolate the softstart from the line as well as the contactor would have to be rated for full voltage bypass.

CTA-ID : 7450
Was this helpful?
What can we do to improve the information ?