Technical FAQs

Ask a Question

What torque is required for the wire binding screw for the AL2500PA lug for P frame breakers (PA, PH, PC, PE, PX)?

46 lb-ft or 62 N-M


CTA-ID : 9087
Was this helpful?
What can we do to improve the information ?