Technical FAQs

Ask a Question

What wire sizes will the AL1200NE6 lug for NA, NC, NE, NX breakers accept?

(4) 3/0 AWG-600 kcmil or 95-300 mm2




CTA-ID : 9083
Was this helpful?
What can we do to improve the information ?