Technical FAQs

Ask a Question

What is the required wire-binding screw torque for the AL1200NE6T lug for NA, NC, NE, NX breakers?

330 lb-in or 38 N-M


CTA-ID : 9080
Was this helpful?
What can we do to improve the information ?