Technical FAQs

Ask a Question

How many Altistart ATS46 starters can be on a Modbus connection?

The maximum number of nodes is 32 including the master.
This would limit the number of soft starters to a maximum of 31 per network.

CTA-ID : 7447
Was this helpful?
What can we do to improve the information ?