Technical FAQs

Ask a Question

What do you need to select an Altistart ATS46 on a 3600 rpm motor?

Issue: What do you need to select an Altistart ATS46 on a 3600 rpm motor?
 
Product Line: ATS46
 
Environment: All
 
Cause: N/A
 
Resolution: Size based on motor Full load current.


 
Was this helpful?
What can we do to improve the information ?