Technical FAQs

Ask a Question

Why would someone use a class 20 overload vs class 10 overload when set up the Altistart ATS46?

A class 10 overload is used in standard duty and class 20 is used for heavy duty.

CTA-ID : 7390
Was this helpful?
What can we do to improve the information ?