Technical FAQs

Ask a Question

How can you get Altivar ATV16 to hold in place without using mechanical holding brake?

Issue: How can you get Altivar ATV16 to hold motor in place without using mechanical holding brake?
 
Product Line: ATV16
 
Environment: All
 
Cause: N/A
 
Resolution: The ATV16 Can`t produce 100% torque at zero speed so the drive will not work in this type application.


 
Was this helpful?
What can we do to improve the information ?