Technical FAQs

Ask a Question

What enclosures are available for the walking beam mechanical interlock systems?

Fully enclosed interlock units are available in Type 1 and Type 3R enclosures, with two neutrals provided in each enclosure. The complete enclosed assembly is not UL listed.


CTA-ID : 9074
Was this helpful?
What can we do to improve the information ?