Technical FAQs

Ask a Question

What type of circuit breakers are used for disconnecting means for the enclosed 8639 Altstart ATS46?

Issue: What type of circuit breakers are used for disconnecting means for the enclosed 8639 Altstart ATS46?
 
Product Line: Enclosed ATS46
 
Environment: 8639 enclosed ATS46
 
Cause: N/A
 
Resolution: They are thermal magnetic breakers
They are FAL, KAL, LAL or MAL type depending on the size of the unit.
See page 15 of Catalog No. 8636CT9701R2/00 August 2000 for details.


 
Was this helpful?
What can we do to improve the information ?