Technical FAQs

Ask a Question

How do you wire a 3 wire 2.5 k ohm speed potentiometer on the Altivar ATV16 ATV18 ATV28 ATV31 ATV56 ATV66?

Issue: How do you wire a 3 wire 2.5 k ohm speed potentiometer on the Altivar ATV16 ATV18 ATV28 ATV31 ATV56 ATV66?
 
Product Line: ATV16 ATV18 ATV28 ATV56 ATV31 ATV66
 
Environment: All
 
Cause: N/A
 
Resolution: Need to wire terminal 1 to COM, terminal 2 ( wiper ) to AI1(AIV for ATV16) and terminal 3 to +10.


 
Was this helpful?
What can we do to improve the information ?