Technical FAQs

Ask a Question

Is the ammeter standard on the LX36600G breaker?

No. It is optional, use part number ALAM. The ammeter is standard on the LE, ME, PE, NE and SE.


CTA-ID : 1962
Was this helpful?
What can we do to improve the information ?