Technical FAQs

Ask a Question

How do you get the Altivar ATV16 unit to ramp to 60hz as soon as power applied and don`t need speed variation currently.

Issue: How do you get the Altivar ATV16 unit to ramp to 60hz as soon as power applied and don`t need speed variation currently.
 
Product Line: ATV16
 
Environment: All
 
Cause: N/A
 
Resolution: Set up for 2-wire standard instead transistional control and informed of the switch 1 positioning (set hz to 50hz) as well as the parameters ( tFr, FrS & UnS ) that needed to be reset and instructed with the jumpers he has between 24v and fwd along with 10v to AIV unit should have unit ramp up to full speed when power is applied.


 
Was this helpful?
What can we do to improve the information ?