Technical FAQs

Ask a Question

How can customer get a dry contact to indicate the Altivar ATV16 drive is running?

Issue: How can customer get a dry contact to indicate the Altivar ATV16 drive is running?
 
Product Line: ATV16
 
Environment: All
 
Cause: N/A
 
Resolution: Need an option card to get a Logic output to change state when drive is running. The option card is VW3A16204 (General use 3-wire control).


 
Was this helpful?
What can we do to improve the information ?