Technical FAQs

Ask a Question

Customer has a HOM250GFI on a 240v 2 wire circuit and needs to know if it will work properly.

It will if wired per instructions. Since there is no load neutral conductor, leave the load neutral connection on the breaker empty. Still must connect the pigtail to grounded panel neutral. The same is true for the QO-GFI


CTA-ID : 5412
Was this helpful?
What can we do to improve the information ?