Technical FAQs

Ask a Question

Are all motors to have a 90 degree phase difference between voltage and current when used with Altistart ATS23?

Issue:   Are all motors to have a 90 degree phase difference between voltage and current when used with Altistart ATS23?
 
Product Line:   ATS23
 
Environment:  All

Cause:   N/A
 
Resolution:   Must have a .95 lagging power factor--current must lag voltage.


 
Was this helpful?
What can we do to improve the information ?