Technical FAQs

Ask a Question

What is the operating temperature for the Altivar ATV16 unit?

Issue: What is the operating temperature for the Altivar ATV16 unit?
 
Product Line: ATV16
 
Environment: All
 
Cause: N/A
 
Resolution: The operating temperature is 0 to +40 degrees C with top plate installed, 0 to +50 degrees C without top plate.


 
Was this helpful?
What can we do to improve the information ?