Technical FAQs

Ask a Question

What does it mean when the the forward light is blinking on the Altivar ATV16?

Issue: What does it mean when the the forward light is blinking on the Altivar ATV16?
 
Product Line: ATV16
 
Environment: All
 
Cause: FWD LED blinking
 
Resolution: This is when you have a forward command but do not have a speed command.


 
Was this helpful?
What can we do to improve the information ?