Technical FAQs

Ask a Question

Why do you not see the LFr parameter to control in keypad mode and has Altivar ATV16 with keypad VW3A16102?

Issue: Why do you not see the LFr parameter to control in keypad mode and has Altivar ATV16 with keypad VW3A16102?
 
Product Line: ATV16
 
Environment: All
 
Cause: No LFR parameter
 
Resolution: The LFr parameter does not appear if the keypad part number VW3A16102 (which is required) datecode is before 9422.


 
Was this helpful?
What can we do to improve the information ?