Technical FAQs

Ask a Question

How is a HRK60 Class R Fuse Kit assembled to the switch fuse clips?

Product Feature

Product Line:
HD SS Accessory

Clarification of design feature

The HRK60 adapters barbed end is pushed firmly into a slot in the base near the fuse clips. This slot may be located near the LINE side or the LOAD side fuse clips of the switch, dependent upon the specific switch. Identify whether the adaptor goes on the Line or Load end of the base by locating this hole in the base. The circular portion of the adapter should engage a slot in the fuse clip. The adapter should not be able to be removed once properly installed. Three adapters are included in each kit.

CTA-ID : 1748
Was this helpful?
What can we do to improve the information ?