Technical FAQs

Ask a Question

Can the QO GFI be used at 50Hz?

No. The QO GFI is UL listed for 60 Hz applications only. At 50 Hz the trip range will be higher and it will not meet UL listing requirements.


CTA-ID : 2130
Was this helpful?
What can we do to improve the information ?