Technical FAQs

Ask a Question

Assistance wiring an HOM220GFI on a 240 volt only circuit

  1. The two hots go to load
  2. Pig tail on breaker goes to grounded neutral bar in panel
  3. Load ground wire to panel ground
  4. Press test button to check
  5. Load neutral connection on breaker left open if there is no load neutral
Was this helpful?
What can we do to improve the information ?