Technical FAQs

Ask a Question

Can I use a QO 2 pole GFI for a combination of 240 vac and 120 vac loads?

Yes, as long as the neutral for the 120 Vac loads is connected to the neutral terminal on the breaker and the pigtail is connected to the neutral bar in the panel.


CTA-ID : 999
Was this helpful?
What can we do to improve the information ?