Technical FAQs

Ask a Question

What determines the input current curent rating of the Altivar ATV66 drive?

The input current is dependant upon the AIC of the system. Current distortion is dependant upon the impedance of the system.

CTA-ID : 7193
Was this helpful?
What can we do to improve the information ?