Technical FAQs

Ask a Question

Which pins are transmit and receive in RS485, on the PCMCIA card when using modbus on the Altivar ATV66?

There isn`t transmit and receive in modbus 485, daisy chain DA to DA and DB to DB


CTA-ID : 7180
Was this helpful?
What can we do to improve the information ?