Technical FAQs

Ask a Question

Can the DRR relay contacts operate 120vac on the Omegapak 8804 Type PT/VT with the option card installed?

Yes. The relay is rated 5 amps at 24vdc 120 vac.


CTA-ID : 4176
Was this helpful?
What can we do to improve the information ?