Technical FAQs

Ask a Question

Is the CMI part number 52902-02-020-50 a valid part number for a digital meter to be used with the Omegapak 8804 CT, EVT and VT?

52902-020-50 is a valid part number for a digital meter which were used on Omegapak 8804 units and other units. Faxed bulletin 50006-020-01.


CTA-ID : 4172
Was this helpful?
What can we do to improve the information ?