Technical FAQs

Ask a Question

Customer is looking for a torque values for an FG breaker.

15 to 30 amps - 30 lb-in
35 to 100 amps - #14-#10 AWG Al/Cu - 35 lb-in, #8 - #2/0 AWG Al/Cu - 50 lb-in. See circuit breaker faceplate label or optional lug instructions for wire size and torque.


CTA-ID : 948
Was this helpful?
What can we do to improve the information ?