Technical FAQs

Ask a Question

Will a FAL breaker with a shunt trip, catalog number FAL340801021, will fit into the FA100S enclosure?

Cause:
Product design features

Product Line:
Circuit Breaker Enclosures

Environment:
Breakers with elelctrical accessories

Cause:
Application

Resolution:
Yes. The FAL340801021 breaker with shunt trip will mount into the FA100S. The Shunt trip is mounted internally to the breaker at the factory and does not change the breaker mounting dimensions.


CTA-ID : 1980
Was this helpful?
What can we do to improve the information ?