Technical FAQs

Ask a Question

Is the Altivar ATV66 capable of communicating w/ Profibus?

It can communicate with Profibus but need to go thru 3rd party Panel Tec @ 1-800-869-2026 to obtain interface unit.


CTA-ID : 7155
Was this helpful?
What can we do to improve the information ?