Technical FAQs

Ask a Question

Is version 2.0 Altivar ATV66 control basket incompatible with VW3A66202, I/O Extension module?

Yes, he will need to upgrade the control basket. A control basket from and ATV66U72N4 will work.


CTA-ID : 7148
Was this helpful?
What can we do to improve the information ?