Technical FAQs

Ask a Question

Can you use current limit to prevent the Altivar ATV66 drive from tearing up a conveyor?

Yes, As long as the current limit is not set too low to prevent you from starting the conveyor. If it is , can set current limit by frequency level.


CTA-ID : 7108
Was this helpful?
What can we do to improve the information ?