Technical FAQs

Ask a Question

Can you assign a logic output to fault state other than the R1 which is allready assigned to a fault on the Altivar ATV66?

In menu 7.3 you can assign logic output to fault state and if in fault state, logic output is high or relay is energized. The R1 relay deenergizes upon fault.

CTA-ID : 7101
Was this helpful?
What can we do to improve the information ?