Technical FAQs

Ask a Question

Is there an output contact based on undercurrent situation in the Altivar ATV66?

Told him he could use the current level which will give a logic output if the current goes above a certain preset value which would program in menu 7.3. This works the opposite direction but a PLC can interpret the data.

CTA-ID : 7096
Was this helpful?
What can we do to improve the information ?