Technical FAQs

Ask a Question

What is the Electrical Interlock Kit for a H60XFA, Series E1 Enclosed Molded Case Switch?

Issue:
product design features

Product line:
Enclosed molded case switches

Resolution:
An Electrical Interlock Kit is not available. A factory installed auxiliary switch can be provided. Order H60XFA1212 for the device to be provided with factory installed 1NO/1NC auxiliary switches. Order H60XFA1352 for the device to be provided with factory installed 2NO/2NC auxiliary switches.


CTA-ID : 8943
Was this helpful?
What can we do to improve the information ?